PMIC_POR and PORESET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC_POR and PORESET

Jump to solution
1,691 Views
trondwang
Contributor I

Hi NXP,

referring to reset circuit in the schematic of your reference design from Embedded Planet, DES0541_11; page 2:

PMIC_POR_B is connected to R60, but R60 is NOPOP so it will not enter MR_b input of the reset circuit U9.

Instead, PMIC_POR is bypassing the reset circuit through R63 into AND-gate U12 and anded with the RST_ output from U9.

Is there any particular reason why PMIC_POR is bypassing the reset circuit U9?

Could PMIC_POR be connected to MR_b through R60 and instead R63 be NOPOP?

regards Trond Inge 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,566 Views
alexander_yakov
NXP Employee
NXP Employee

I do not see a significant difference between PMIC_POR_B connected to U9 and to U12. The difference is only in 140ms duration generated by MIC2774N in response to MR input assertion. As per my understanding, connecting to U9 is not necessary in this case, PMIC itself generates proper timing, so direct connection via AND gate U12 is enough.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,567 Views
alexander_yakov
NXP Employee
NXP Employee

I do not see a significant difference between PMIC_POR_B connected to U9 and to U12. The difference is only in 140ms duration generated by MIC2774N in response to MR input assertion. As per my understanding, connecting to U9 is not necessary in this case, PMIC itself generates proper timing, so direct connection via AND gate U12 is enough.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------