Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0

Jump to solution
3,718 Views
skrishnakar
Contributor III

Hello All,

I have been trying to boot the LS1021A-TWR board with Qoriq SDK v2.0 and been seeing this network driver crash there after the NFS boot hangs:

-------------snip----------------

Key type dns_resolver registered

Registering SWP/SWPB emulation handler

sgtl5000 1-000a: Using internal LDO instead of VDDD

asoc-simple-card sound: sgtl5000 <-> 2b50000.sai mapping ok

hctosys: unable to open rtc device (rtc0)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

random: nonblocking pool is initialized

IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready

IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready

fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx

IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready

Sending DHCP requests ..

------------[ cut here ]------------

WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:321 dev_watchdog+0x1d8/0x260()

NETDEV WATCHDOG: eth1 (fsl-gianfar): transmit queue 0 timed out

Modules linked in:

CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.1.8-rt8+ls1+gbd51baf #2

Hardware name: Freescale LS1021A

[<80025508>] (unwind_backtrace) from [<800222c0>] (show_stack+0x10/0x14)

[<800222c0>] (show_stack) from [<8056e888>] (dump_stack+0x70/0x8c)

[<8056e888>] (dump_stack) from [<8003cbc8>] (warn_slowpath_common+0x80/0xac)

[<8003cbc8>] (warn_slowpath_common) from [<8003cc20>] (warn_slowpath_fmt+0x2c/0x3c)

[<8003cc20>] (warn_slowpath_fmt) from [<804806c4>] (dev_watchdog+0x1d8/0x260)

[<804806c4>] (dev_watchdog) from [<8007e69c>] (call_timer_fn+0x20/0x90)

[<8007e69c>] (call_timer_fn) from [<8007e9a8>] (run_timer_softirq+0x1d8/0x218)

[<8007e9a8>] (run_timer_softirq) from [<8003fe68>] (__do_softirq+0xd4/0x200)

[<8003fe68>] (__do_softirq) from [<80040558>] (irq_exit+0x84/0xf4)

[<80040558>] (irq_exit) from [<800712ac>] (__handle_domain_irq+0x90/0xb4)

[<800712ac>] (__handle_domain_irq) from [<80009444>] (gic_handle_irq+0x3c/0x5c)

[<80009444>] (gic_handle_irq) from [<80573000>] (__irq_svc+0x40/0x54)

Exception stack(0xbf07bf98 to 0xbf07bfe0)

bf80:                                                       00000001 00000000

bfa0: 00000000 8002e360 bf07a000 00000000 30c0387d 00000000 bf07bfe8 807ac418

bfc0: 00000001 00000000 01000000 bf07bfe0 8001fd74 8001fd78 60000113 ffffffff

[<80573000>] (__irq_svc) from [<8001fd78>] (arch_cpu_idle+0x2c/0x38)

[<8001fd78>] (arch_cpu_idle) from [<80069c30>] (cpu_startup_entry+0x22c/0x26c)

[<80069c30>] (cpu_startup_entry) from [<8000950c>] (__enable_mmu+0x0/0x14)

---[ end trace f274e2c156a0521b ]---

fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx

.

fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx

.

fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx

---------------8<-------------------

Could anyone confirm that network driver is working without any issues in Qoriq SDK v2.0 for Layerscape LS1021A board ?

Thanks in Advance!

-skrishna

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,762 Views
skrishnakar
Contributor III

All images of u-boot, rcw and kernel 4.1.8-rt8 are booting fine and network driver is also working fine on TWR-LS1021A-PB Rev 2.0.

View solution in original post

0 Kudos
Reply
10 Replies
2,763 Views
skrishnakar
Contributor III

All images of u-boot, rcw and kernel 4.1.8-rt8 are booting fine and network driver is also working fine on TWR-LS1021A-PB Rev 2.0.

0 Kudos
Reply
2,762 Views
xkonni
Contributor II

same happens for me.

here's a (hopefully) complete bootlog:

=> run sdboot

reading uImage

3510824 bytes read in 166 ms (20.2 MiB/s)

reading ls1021a-twr.dtb

21610 bytes read in 18 ms (1.1 MiB/s)

reading rootfs

53187597 bytes read in 2257 ms (22.5 MiB/s)

## Booting kernel from Legacy Image at 81000000 ...

   Image Name:   Linux-4.1.8-rt8+gbd51baf

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3510760 Bytes = 3.3 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 88000000 ...

   Image Name:   fsl-image-mesh-ls1021atwr-201606

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    53187533 Bytes = 50.7 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 8f000000

   Booting using the fdt blob at 0x8f000000

   Loading Kernel Image ... OK

   Loading Ramdisk to bbc4c000, end bef053cd ... OK

   Loading Device Tree to bbc43000, end bbc4b469 ... OK

Starting kernel ...

Booting Linux on physical CPU 0xf00

Linux version 4.1.8-rt8+gbd51baf (jenkins@mercury) (gcc version 4.9.3 20150311 (prerelease) (Linaro GCC 4.9-2015.03) ) #1 SMP Sun May 15 05:05:43 CST 2016

CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=70c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: LS1021A TWR Board

Forcing write-allocate cache policy for SMP

Memory policy: Data cache writealloc

PERCPU: Embedded 12 pages/cpu @bffcd000 s16640 r8192 d24320 u49152

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: root=/dev/ram0 rw console=ttyS0,115200 hdmi high

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 979732K/1048576K available (3695K kernel code, 224K rwdata, 1752K rodata, 236K init, 209K bss, 68844K reserved, 0K cma-reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f800000 - 0x7fe00000   (   6 MB)

      .text : 0x80008000 - 0x8055a1bc   (5449 kB)

      .init : 0x8055b000 - 0x80596000   ( 236 kB)

      .data : 0x80596000 - 0x805ce358   ( 225 kB)

       .bss : 0x805d1000 - 0x80605694   ( 210 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

Hierarchical RCU implementation.

[8CAdditional per-CPU info printed with stalls.

[8CRCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2

NR_IRQS:16 nr_irqs:16 16

Architected cp15 timer(s) running at 12.50MHz (phys).

clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049cda, max_idle_ns: 440795202628 ns

sched_clock: 56 bits at 12MHz, resolution 80ns, wraps every 4398046511080ns

Switching to timer-based delay loop, resolution 80ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 25.00 BogoMIPS (lpj=125000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

CPU: Testing write buffer coherency: ok

CPU0: update cpu_capacity 1024

CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00

Setting up static identity map for 0x80008280 - 0x800082e4

CPU1: update cpu_capacity 1024

CPU1: thread -1, cpu 1, socket 15, mpidr 80000f01

Brought up 2 CPUs

SMP: Total of 2 processors activated (50.00 BogoMIPS).

CPU: All CPU(s) started in HYP mode.

CPU: Virtualization extensions available.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

irq: no irq domain found for /soc/uqe@2400000/qeic@80 !

irq: no irq domain found for /soc/uqe@2400000/qeic@80 !

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

register e1000-wakeup irq error, ret = -22

Serial: AMBA PL011 UART driver

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource arch_sys_counter

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 51944K (bbc4c000 - bef06000)

kvm [1]: interrupt-controller@1404000 IRQ22

kvm [1]: timer IRQ18

kvm [1]: Hyp mode initialized successfully

CPU PMU: Failed to parse /pmu/interrupt-affinity[0]

hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available

futex hash table entries: 512 (order: 3, 32768 bytes)

HugeTLB registered 2 MB page size, pre-allocated 0 pages

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

PCI host bridge /soc/pcie@3400000 ranges:

   IO 0x4000010000..0x400001ffff -> 0x00000000

  MEM 0x4040000000..0x407fffffff -> 0x40000000

layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [bus 00-ff]

pci_bus 0000:00: root bus resource [io  0x0000-0xffff]

pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0000:00:00.0: BAR 1: assigned [mem 0x4040000000-0x4043ffffff]

pci 0000:00:00.0: BAR 0: assigned [mem 0x4044000000-0x4044ffffff]

pci 0000:00:00.0: BAR 6: assigned [mem 0x4045000000-0x4045ffffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

PCI host bridge /soc/pcie@3500000 ranges:

   IO 0x4800010000..0x480001ffff -> 0x00000000

  MEM 0x4840000000..0x487fffffff -> 0x40000000

layerscape-pcie 3500000.pcie: PCI host bridge to bus 0001:00

pci_bus 0001:00: root bus resource [bus 00-ff]

pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x0000-0xffff])

pci_bus 0001:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0001:00:00.0: BAR 1: assigned [mem 0x4840000000-0x4843ffffff]

pci 0001:00:00.0: BAR 0: assigned [mem 0x4844000000-0x4844ffffff]

pci 0001:00:00.0: BAR 6: assigned [mem 0x4845000000-0x4845ffffff pref]

pci 0001:00:00.0: PCI bridge to [bus 01]

Sii902x: read id = 0xB0

-0x02-0x03

-0x00

sii902x 1-0039: Can not read edid

Console: switching to colour frame buffer device 60x34

fb0: fb device registered successfully.

fb1: fb device registered successfully.

fb2: fb device registered successfully.

fb3: fb device registered successfully.

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

console [ttyS0] disabled

21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 34, base_baud = 9375000) is a 16550A

console [ttyS0] enabled

21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 34, base_baud = 9375000) is a 16550A

sii902x 1-0039: read edid fail

2950000.serial: ttyLP0 at MMIO 0x2950000 (irq = 40, base_baud = 6250000) is a FSL_LPUART

fsl-lpuart 2950000.serial: DMA tx channel request failed, operating without tx DMA

fsl-lpuart 2950000.serial: DMA rx channel request failed, operating without rx DMA

brd: module loaded

loop: module loaded

/soc/sata@3200000: could not get #clock-cells for /soc/clocking@1ee1000

ahci-qoriq 3200000.sata: AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl platform mode

ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc

ahci-qoriq 3200000.sata: port 0 is not capable of FBS

scsi host0: ahci-qoriq

ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 27

60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e

Amd/Fujitsu Extended Query Table at 0x0040

  Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

10 ofpart partitions found on MTD device 60000000.nor

Creating 10 MTD partitions on "60000000.nor":

0x000000000000-0x000000020000 : "NOR bank0 RCW Image"

0x000000100000-0x000000200000 : "NOR bank0 u-boot Image"

0x000000200000-0x000000300000 : "NOR bank0 DTB Image"

0x000000300000-0x000000a00000 : "NOR bank0 Linux Kernel Image"

0x000000a00000-0x000004000000 : "NOR bank0 Ramdisk Root File System Image"

0x000004000000-0x000004020000 : "NOR bank4 RCW Image"

0x000004100000-0x000004200000 : "NOR bank4 u-boot Image"

0x000004200000-0x000004300000 : "NOR bank4 DTB Image"

0x000004300000-0x000004a00000 : "NOR bank4 Linux Kernel Image"

0x000004a00000-0x000008000000 : "NOR bank4 Ramdisk Root File System Image"

fsl-quadspi 1550000.quadspi: unrecognized JEDEC id bytes: 00, 00, 00

fsl-quadspi 1550000.quadspi: Freescale QuadSPI probe failed

fsl-quadspi: probe of 1550000.quadspi failed with error -2

m25p80 spi0.0: unrecognized JEDEC id bytes: 00, 00, 00

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

2a70000.can supply xceiver not found, using dummy regulator

flexcan 2a70000.can: device registered (reg_base=c08bc000, irq=49)

2a80000.can supply xceiver not found, using dummy regulator

flexcan 2a80000.can: device registered (reg_base=c08be000, irq=50)

libphy: Freescale PowerQUICC MII Bus: probed

fsl-gianfar soc:ethernet@2d10000: enabled errata workarounds, flags: 0x4

fsl-gianfar soc:ethernet@2d10000 eth0: mac: 00:04:9f:03:f5:b1

fsl-gianfar soc:ethernet@2d10000 eth0: Running with NAPI enabled

fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[1]: 256

fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[1]: 256

fsl-gianfar soc:ethernet@2d50000: enabled errata workarounds, flags: 0x4

fsl-gianfar soc:ethernet@2d50000 eth1: mac: 00:04:9f:03:f5:b2

fsl-gianfar soc:ethernet@2d50000 eth1: Running with NAPI enabled

fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[1]: 256

fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[1]: 256

fsl-gianfar soc:ethernet@2d90000: enabled errata workarounds, flags: 0x4

fsl-gianfar soc:ethernet@2d90000 eth2: mac: 00:04:9f:03:f5:b3

fsl-gianfar soc:ethernet@2d90000 eth2: Running with NAPI enabled

fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[1]: 256

fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[0]: 256

fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[1]: 256

pps pps0: new PPS source ptp0

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2014 Intel Corporation.

ata1: SATA link down (SStatus 0 SControl 300)

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1

xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66c hci version 0x100 quirks 0x00010010

xhci-hcd xhci-hcd.0.auto: irq 52, io mem 0x03100000

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2

usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

mousedev: PS/2 mouse device common for all mice

i2c /dev entries driver

ina2xx 0-0040: power monitor ina220 (Rshunt = 1000 uOhm)

ina2xx 0-0041: power monitor ina220 (Rshunt = 1000 uOhm)

0-004c supply vcc not found, using dummy regulator

lm90 0-004c: Register 0x4 read failed (-5)

lm90 0-004c: Failed to read convrate register!

lm90 0-004c: Register 0x3 read failed (-5)

lm90 0-004c: Initialization failed!

imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0)

qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-esdhc 1560000.esdhc: No vmmc regulator found

sdhci-esdhc 1560000.esdhc: No vqmmc regulator found

mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit

caam 1700000.crypto: Instantiated RNG4 SH1

caam 1700000.crypto: device ID = 0x0a14030000000000 (Era 7)

caam 1700000.crypto: job rings = 4, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 1710000.jr: registering rng-caam

caam 1700000.crypto: fsl,sec-v5.0 algorithms registered in /proc/crypto

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

sgtl5000 1-000a: sgtl5000 revision 0x11

oprofile: using timer interrupt.

Initializing XFRM netlink socket

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

Key type dns_resolver registered

Registering SWP/SWPB emulation handler

sgtl5000 1-000a: Using internal LDO instead of VDDD

mmc0: new high speed SDHC card at address e624

mmcblk0: mmc0:e624 SL08G 7.40 GiB

mmcblk0: p1 p2 p3

asoc-simple-card sound: sgtl5000 <-> 2b50000.sai mapping ok

hctosys: unable to open rtc device (rtc0)

ALSA device list:

  #0: 2b50000.sai-sgtl5000

RAMDISK: gzip image found at block 0

random: nonblocking pool is initialized

RAMDISK: incomplete write (-28 != 32768)

write error

VFS: Mounted root (ext2 filesystem) on device 1:0.

devtmpfs: mounted

Freeing unused kernel memory: 236K (8055b000 - 80596000)

INIT: version 2.88 booting

EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)

Starting udev

udevd[163]: starting version 182

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

Populating dev cache

udev-cache: update failed!

hwclock: can't open '/dev/misc/rtc': No such file or directory

Tue Jun 14 12:03:56 UTC 2016

hwclock: can't open '/dev/misc/rtc': No such file or directory

update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)

Removing any system startup links for run-postinsts ...

  /etc/rcS.d/S99run-postinsINIT: Entering runlevel: 5

Configuring network interfaces... udhcpc (v1.23.2) started

Sending discover...

Sending discover...

fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx

Sending discover...

No lease, forking to background

done.

Starting OpenBSD Secure Shell server: sshd

  generating ssh RSA key...

hwclock: can't open '/dev/misc/rtc': No such file or directory

Starting syslogd/klogd: done

Poky (Yocto Project Reference Distro) 2.0.2 ls1021atwr /dev/ttyS0

ls1021atwr login: ------------[ cut here ]------------

WARNING: CPU: 0 PID: 0 at /home/jenkins/ci/sdk/master/ls1021atwr/sources/linux/net/sched/sch_generic.c:318 dev_watchdog+0x153/0x1b4()

NETDEV WATCHDOG: eth0 (fsl-gianfar): transmit queue 1 timed out

Modules linked in:

CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.8-rt8+gbd51baf #1

Hardware name: Freescale LS1021A

[<8001d17d>] (unwind_backtrace) from [<8001ad13>] (show_stack+0xb/0xc)

[<8001ad13>] (show_stack) from [<80370741>] (dump_stack+0x51/0x64)

[<80370741>] (dump_stack) from [<8002f811>] (warn_slowpath_common+0x55/0x7c)

[<8002f811>] (warn_slowpath_common) from [<8002f853>] (warn_slowpath_fmt+0x1b/0x24)

[<8002f853>] (warn_slowpath_fmt) from [<8030895f>] (dev_watchdog+0x153/0x1b4)

[<8030895f>] (dev_watchdog) from [<8005c097>] (call_timer_fn.isra.28+0x15/0x5e)

[<8005c097>] (call_timer_fn.isra.28) from [<8005c707>] (run_timer_softirq+0x131/0x162)

[<8005c707>] (run_timer_softirq) from [<80031b91>] (__do_softirq+0x99/0x164)

[<80031b91>] (__do_softirq) from [<80032037>] (irq_exit+0x4b/0x9c)

[<80032037>] (irq_exit) from [<8005357b>] (__handle_domain_irq+0x57/0x74)

[<8005357b>] (__handle_domain_irq) from [<80009329>] (gic_handle_irq+0x29/0x40)

[<80009329>] (gic_handle_irq) from [<8037391b>] (__irq_svc+0x3b/0x5c)

Exception stack(0x80597f58 to 0x80597fa0)

7f40:                                                       00000001 00000000

7f60: 00000000 800238a1 80596000 00000000 00000000 80597fa8 8059041c 00000001

7f80: 80584850 00000000 80598180 80597fa0 80019351 80019352 40070033 ffffffff

[<8037391b>] (__irq_svc) from [<80019352>] (arch_cpu_idle+0x14/0x1e)

[<80019352>] (arch_cpu_idle) from [<8004e4d7>] (cpu_startup_entry+0x173/0x1ac)

[<8004e4d7>] (cpu_startup_entry) from [<8055b913>] (start_kernel+0x273/0x2dc)

---[ end trace 2203d1c056f202bb ]---

fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx

fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx

fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx

fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx

Poky (Yocto Project Reference Distro) 2.0.2 ls1021atwr /dev/ttyS0

0 Kudos
Reply
2,762 Views
xkonni
Contributor II

bump.

this is quite a serious issue. could someone please look into this?

thanks!

0 Kudos
Reply
2,762 Views
ufedor
NXP Employee
NXP Employee

Please provide corresponding U-Boot log.

0 Kudos
Reply
2,762 Views
xkonni
Contributor II

sure, just created a fresh one (rootfs, uimage, dtb directly from sdk2.0).

thanks for your help!

0 Kudos
Reply
2,762 Views
ufedor
NXP Employee
NXP Employee

Were you using SDK 2.0 pre-built images?

If "not" - what were the kernel build options?

0 Kudos
Reply
2,762 Views
xkonni
Contributor II

Yes this log was with the pre-built sdk uImage, dtb, rootfs.

But custom images with a slightly modified ls1021a_defconfig, yocto sdk2 branch lead to the same issue.

0 Kudos
Reply
2,762 Views
ufedor
NXP Employee
NXP Employee

Please check the board switch settings - what are they?

0 Kudos
Reply
2,762 Views
xkonni
Contributor II

SW2[1:8] = 0010 1111

SW3[1:8] = 0110 0001

like described in the demo pdf.

but apparently the issue was that I didnt flash the new u-boot to the sdcard. issue seems resolved.

0 Kudos
Reply
2,762 Views
ufedor
NXP Employee
NXP Employee

Please provide U-Boot log for the board.