MK20DX128VFM5 must required for LS1012A programming and debugging?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DX128VFM5 must required for LS1012A programming and debugging?

2,254 次查看
nilavchoksi
Contributor III

Hi NXP Team,

 

Please confirm that MK20DX128VFM5(CMSIS DAP) must require for programming and debugging of LS1012A?

 

I am planning to program and debug it through direct 10-pin JTAG Header so is it OK?

 

Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?

This CMSIS-DAP is used in all reference designs of LS1012A, so please clear this doubt and share interface diagram.

标签 (1)
6 回复数

2,068 次查看
shyam_baldha
Contributor I

Hi ufedor,

Can we use CMSIS DAP to program a completely fresh FRDM-ls1012a??

Note: Completely fresh means,empty flash with out any binaly(u-boot, RCW, kernel image).

Since we are designing an custom board referring FRDM-LS1012A, We will be needed to program a completely empty flash. So I wants to know the possible interfaces/procedure to program fresh flash.

If it is not possible using with CMSIS DAP, What could be the other option do we have??

Thanks,

Shyam

0 项奖励
回复

2,068 次查看
ufedor
NXP Employee
NXP Employee

> Can we use CMSIS DAP to program a completely fresh FRDM-ls1012a??

No.

CodeWarrior can do that.

0 项奖励
回复

2,068 次查看
ufedor
NXP Employee
NXP Employee

> Please confirm that MK20DX128VFM5(CMSIS DAP) must require for programming and debugging of LS1012A?

The MK20DX128VFM5(CMSIS DAP) is optional.

 

> I am planning to program and debug it through direct 10-pin JTAG Header so is it OK?

This is OK.

 

> Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?

The MK20DX128VFM5(CMSIS DAP) is a low-cost debug option.

When CodeWarrior TAP is not used the CodeWarrior could use CMSIS DAP to establish debug connection. Drawback of the CMSIS DAP approach is its significant slowness in comparison to the CodeWarrior TAP.

2,068 次查看
nilavchoksi
Contributor III

Hi,

Can you please explain the difference between CodeWarrior TAP and CMSIS DAP.

Also, How CodeWarrior TAP is more useful to debug more faster for processor?

Can I use FTDI chip to debug LS1012A processor?

0 项奖励
回复

2,068 次查看
ufedor
NXP Employee
NXP Employee

> Can you please explain the difference between CodeWarrior TAP and CMSIS DAP.

These are different access ports.

CodeWarrior TAP:

CodeWarrior TAP|NXP 

CMSIS DAP:

CMSIS DAP - Handbook | mbed 

> Also, How CodeWarrior TAP is more useful to debug more faster for processor?

The CodeWarrior TAP has significantly more complicated hardware.

> Can I use FTDI chip to debug LS1012A processor?

No support from NXP is provided.

0 项奖励
回复

2,068 次查看
nilavchoksi
Contributor III

Hi,

Thank you for reply and guide us.

0 项奖励
回复