Ls1043a configure SGMII@MAC9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ls1043a configure SGMII@MAC9

1,205件の閲覧回数
chcmedeiros
Contributor I

Hello,

I'm currently working on a custom board with LS1043a. This board has the following connection:

chcmedeiros_0-1645458981236.png

We are using Uboot 2020.04 and Linux  5.4.47. Our serdes protocol is 0x3555.

At this  point we are able to ping an external PC on Uboot (the SERDES PLL reset was necessary), but when reaching Linux we are not able to ping an external device (even when we re-send the PLL reset command), not sure if this is a device tree problem.

I added in the attachments my device tree, uboot log and kernel log, if someone had a similar concern and can give me any hint.

ラベル(2)
タグ(3)
0 件の賞賛
1 返信

1,201件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide connection schematics as PDF and measured frequencies of the SerDes reference clocks.

0 件の賞賛