Ls1043a configure SGMII@MAC9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ls1043a configure SGMII@MAC9

1,121 Views
chcmedeiros
Contributor I

Hello,

I'm currently working on a custom board with LS1043a. This board has the following connection:

chcmedeiros_0-1645458981236.png

We are using Uboot 2020.04 and Linux  5.4.47. Our serdes protocol is 0x3555.

At this  point we are able to ping an external PC on Uboot (the SERDES PLL reset was necessary), but when reaching Linux we are not able to ping an external device (even when we re-send the PLL reset command), not sure if this is a device tree problem.

I added in the attachments my device tree, uboot log and kernel log, if someone had a similar concern and can give me any hint.

Labels (2)
Tags (3)
0 Kudos
1 Reply

1,117 Views
ufedor
NXP Employee
NXP Employee

Please provide connection schematics as PDF and measured frequencies of the SerDes reference clocks.

0 Kudos