Ls1028a displayport support in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ls1028a displayport support in u-boot

1,224件の閲覧回数
stepan_m
Contributor I

Hello. Is there a displayport driver support for ls1028a baremetal defconfig in u-boot? Goal is to get diplay working in u-boot. Tried a bunch of options in menuconfig in graphics support, but it didn't work for me. 
Thanks.

0 件の賞賛
返信
1 返信

1,146件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP LSDK does not support the LS1028a display port under u-boot. NXP LSDK supports the LS1028a display port under Linux.

The LCD and Display Transmitter Controller device drivers can be built in the kernel image or built as kernel modules.

See LSDK User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.04.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------