Ls1028a displayport support in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ls1028a displayport support in u-boot

1,158 Views
stepan_m
Contributor I

Hello. Is there a displayport driver support for ls1028a baremetal defconfig in u-boot? Goal is to get diplay working in u-boot. Tried a bunch of options in menuconfig in graphics support, but it didn't work for me. 
Thanks.

0 Kudos
Reply
1 Reply

1,080 Views
Pavel
NXP Employee
NXP Employee

NXP LSDK does not support the LS1028a display port under u-boot. NXP LSDK supports the LS1028a display port under Linux.

The LCD and Display Transmitter Controller device drivers can be built in the kernel image or built as kernel modules.

See LSDK User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.04.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------