Losing USB3 port on LS1046ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Losing USB3 port on LS1046ARDB

1,184 Views
marco3181
Contributor III

Hello,

When I put an USB3 key on the LS1046A RDB, I lose the port, meaning there are no lights from the LED indicators for the 5V (D1 or D2). Overcurrent? Power Management?

I don't know what to look. The USB is reactivated with a lsusb -v (not the busybox one).

Any hint?

Thank you

Marc

Labels (1)
0 Kudos
Reply
1 Reply

1,066 Views
Pavel
NXP Employee
NXP Employee

It looks like that there is overcurrent on your board if this USB key is connected.Test your board using different USB device (USB memory stick and so on).
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply