Layerscape Hardware Security Module(HSM) storage questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Layerscape Hardware Security Module(HSM) storage questions

跳至解决方案
1,138 次查看
jvfausto
Contributor I

Hello,

In the LSDK User Guide mentions that the SoCs can internally store keys using an HSM. "NXP SoCs such as LS1046A can store keys securely using built-in SoC capabilities - virtual HSM. With such devices, sensitive private keys never leave the device and cryptographic operations are performed on this virtual HSM"(LSDKUG-Rev21.08, CH 6.5.1).

I could not find a reference to whether it is stored using secure non-volatile storage (SNVS), or if it is stored in volatile memory requiring a battery connected such as the with the "Battery Backed Security Monitor supply". Does the SoC need to keep some voltage after powering off to keep the keys stored securely?

And just to confirm, this feature applies to all arm trusted firmware(TFA) enabled CPUs?

标签 (1)
0 项奖励
回复
1 解答
1,058 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @jvfausto 

Hope this post finds you well,

They are stored in a non-volatile memory.

BR,

Hector V

 

在原帖中查看解决方案

2 回复数
1,059 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @jvfausto 

Hope this post finds you well,

They are stored in a non-volatile memory.

BR,

Hector V

 

1,108 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @jvfausto 

Hope this email finds you,

This email is to inform that I keep working on the solution on this case.

I’ll keep you informed on the process,

Have a great day.
 
BR,
Hector Villarruel