Layerscape FRWY-LC1012A board, cannot find parts to build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape FRWY-LC1012A board, cannot find parts to build

1,175 Views
hung_tran
Contributor I

I'm using FRWY-LS1012A as a starting board and I am adding more parts for my custom design. I am trying to source the parts to build this board. But some of parts I can not find the vendor/manufacturer to buy the parts in. Can NXP please help (please also see attached the parts I'm having trouble with). Please let me know where I can buy these parts? 

Thank you,

Hung

ValueReferenceManufacturerP/N
USB3_MICRO_ABJ5CON 10 USB MICRO-AB 3.0 SKT RA SMT 0.65MM SP 106H AUANYTRONIC CORPORATION LIMITED23H90601#LCP-582LF
HDR 2X5J9,J10HDR 2X5 TH 50MIL CTR 167H AU 91LANYTRONIC CORPORATION LIMITED0922S0205011N6T-2LF
23HG0101#LCP-702LFJ11CON 5 USB2.0 MICRO-AB RA REVERSE SKT SMT 0.65MM SP 128H AUANYTRONIC CORPORATION LIMITED23HG0101#LCP-702LF
CON_1X8J33,J34CON 1X8 SKT TH 100MIL SP 344H AU 394LANYTRONIC CORPORATION LIMITED08001S3 0811-100-29LF
M.2 SKTJ35CON 67 PCI EXPRESS M.2 CRD KEY- E SKT RA SMT 0.5MM SP 165H AUANYTRONIC CORPORATION LIMITED1J0E 42010R-2LF
95220030-14RRFJ36CON 8 SKT SD/MMC RA SMT 43MIL SP 84H AUANYTRONIC CORPORATION LIMITED95220030-14RLF
HDR 1X2 THJ37HDR 1X2 TH 100MIL SP 339H AU 98LANYTRONIC CORPORATION LIMITED090021S02015-2LF
3520N811001-14LFJ39CON RJ45 SHLD RA TH 81 SP 593H AU 104LANYTRONIC CORPORATION LIMITED3520N811001-14LF
4.7uHL11,L12IND PWR 4.7uH@1MHZ 1.1A 20% 2020Shenzhen Sunlord Electronics Co., LtdSPH202012H4R7MT
120OHML14,L15,L18,L24,L88IND FER BEAD 120OHM@100MHZ 2A 25% 0603Shenzhen Sunlord Electronics Co., LtdPZ1608U121-2R0TF
W25M161AWEITU11IC MEM FLASH 16M-BIT SERIAL NOR + 1G-BIT SERIAL NAND 1.7-1.95V  WSON-8WINBOND ELECTRONICS CORPW25M161AWEIT
LS1012AU14IC MPU LS1012A 1000MHZ LGA211FREESCALE SEMICONDUCTORLS1012AXE7KKB
AR8033U16,U17IC XCVR ETHERNET PHY 10/100/1000 Mbps 3.3V QFN48Qualcomm Atheros, IncAR8033-AL1A
Tags (1)
0 Kudos
Reply
1 Reply

1,086 Views
ufedor
NXP Employee
NXP Employee

Please use services of Arrow, Octopart or other electronic components suppliers.

0 Kudos
Reply