Latest Available Kernel for LS1043A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Latest Available Kernel for LS1043A

1,330 次查看
sandeepajesh
Contributor III

Hi Guys,

We are working on a LS1043A based board and we want to use latest supported kernel.

Can someone please help me with this. From where I can get latest kernel for LS1043A.

Regards

SS

标签 (1)
1 回复

1,162 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello sandeep sharma,

The latest SDK release for LS1043 is SDK 2.0 1703, you could download ISOs from Linux® SDK for QorIQ ® Processors|NXP.

According to SDK 1703 linux package recipe, the git tree address is as the following.

git://git.freescale.com/ppc/sdk/linux.git

1ae843c08261402b2c35d83422e4fa1e313611f4


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------