[LX2160ARDB] dpni.2 belonging to dprc.2 have no ethernet interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LX2160ARDB] dpni.2 belonging to dprc.2 have no ethernet interface?

1,377件の閲覧回数
wulichang
Contributor I

I'm a new user for NXP LX2160ARDB, also for DPDK programming, my project is using LX2160.

1. current environment already exists dprc.1

When I execute the command, "/usr/local/dpdk/dpaa2/dynamic_dpl.sh dpmac.3"

The result is,

root@localhost:~# ls-listni

dprc.1/dpni.1 (interface: eth0, end point: dpmac.2)
dprc.1/dpni.0 (interface: eth1, end point: dpmac.17)
dprc.1/dprc.2/dpni.2 (end point: dpmac.3)

But I find there's no interface for dpmac.3.

2.If I execute the command after reboot, "ls-addni dpmac.3", not the above command.

root@localhost:~# ls-listni
dprc.1/dpni.1 (interface: eth0, end point: dpmac.2)
dprc.1/dpni.0 (interface: eth1, end point: dpmac.17)
root@localhost:~# ls-addni dpmac.3
Created interface: eth2 (object:dpni.2, endpoint: dpmac.3)
root@localhost:~# ls-listni      
dprc.1/dpni.2 (interface: eth2, end point: dpmac.3)
dprc.1/dpni.1 (interface: eth0, end point: dpmac.2)
dprc.1/dpni.0 (interface: eth1, end point: dpmac.17)

I know there's a difference about dprc, How can do dpni.2 belonging to dprc.2 have a ethernet interface?

ラベル(2)
0 件の賞賛
返信
1 返信

1,138件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Lichang Wu,

dpni.2 belonging  to dprc.2 is assigned to DPDK, so Linux cannot see it(no interface). dprc.1 is assigned to Linux.

Thanks,

Yiping

0 件の賞賛
返信
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----