LX2160ARDB DDR memory access after DDR init

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LX2160ARDB DDR memory access after DDR init

跳至解决方案
4,075 次查看
userland
Contributor II

Hi

After manually initialized the DDR controllers via JTAG I'm trying to access the DDR memory area but it always fails

From what I understand the regions has to be mapped using Trust Zone Address Space Controller, so I've tried doing what u-boot from lsdk2012 did, but I still cannot access the memory region.

A rough step by step how I do it is:

Initialize DDR controller 1 & 2 -> Turn of TZC gatekeeper for each controller -> Apply memory region info ->  set action register -> enable TZC gatekeeper

But the CPU still resets when I try to access the memory region (0x80000000)

0 项奖励
回复
1 解答
4,021 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "class CwPhy(object)" in the attached file.

# Operations
_OPERATIONS = {
'init' : OP_INIT_CONFIG,
'load-firmware' : OP_LOAD_FIRMWARE,
'exec-firmware' : OP_EXEC_FIRMWARE,
'read-message-block' : OP_READ_MESSAGE_BLOCK,
'load-pie' : OP_LOAD_PIE,
'run-diag' : OP_RUN_DIAG
}

 

DDR PHY loads DDR PHY FW at offset 0x00800000 of QSPI flash.

 

在原帖中查看解决方案

3 回复数
4,056 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached CodeWarrior initialization file.

Please refer to the following procedure.

1.  Init_TZASC()

2. Init_DDR_PHY(DDR_freq)

3. Init_DDRC(DDR_freq)

4,039 次查看
userland
Contributor II

Thank you

What exactly does Init_DDR_PHY do?

I'm trying to figure out if it accesses some device registers like TZ and DDRC does

But I guess that DDR PHY loads some kind of firmware?

Why I'm asking is because I'm trying to write a init script for Trace32, so I need to understand all the parts of the process in order to get it to work

Thanks

0 项奖励
回复
4,022 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "class CwPhy(object)" in the attached file.

# Operations
_OPERATIONS = {
'init' : OP_INIT_CONFIG,
'load-firmware' : OP_LOAD_FIRMWARE,
'exec-firmware' : OP_EXEC_FIRMWARE,
'read-message-block' : OP_READ_MESSAGE_BLOCK,
'load-pie' : OP_LOAD_PIE,
'run-diag' : OP_RUN_DIAG
}

 

DDR PHY loads DDR PHY FW at offset 0x00800000 of QSPI flash.