LX2160A second RCW source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LX2160A second RCW source

跳至解决方案
3,463 次查看
dstepanov
Contributor I

Hello! I’m using LX2160A clearfog development board and trying to implement reliable boot in case of failure of one of the boot sources (eMMC/SD/SPI).

LX2160A Reference Manual (Rev. 0RH, 07/2020) in detailed Power-On reset description (4.9.5, table 11, stage 13) points that it is possible to use second RCW source

If the Service processor detects that the RCW loading failed, it initiates RCW loading from a second RCW source. If boot fails from the RCW loaded at offset 0 or 0x1000 (in case of SD), the boot ROM searches for RCW at 8 MB (8 MB + 0x1000 for SD) offset on the device.

I’m little bit confused with this description - what really happens if boot fails? where the second RCW source is selected? Does the boot process try to read RCW from first boot source (using 2 offsets) and if these 2 attempts fails it performs another 2 attempts (with 2 different offsets)?

0 项奖励
回复
1 解答
3,385 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The RM needs to be corrected. There is no second RCW source. This was initially planned but due to certain hardware issues, could not be implemented.

The statement should be removed:
I/O drivers for the backup RCW source are enabled, specifically those pins associated only with the secondary RCW interface.However in LX2160, we do have a provision of secondary RCW source on the same boot device. If boot fails from RCW loaded at offset 0 or 0x1000 ( in case of SD), ROM searches for RCW at 8 MB (8 Mb + 0x1000 for SD) offset on the device.

在原帖中查看解决方案

1 回复
3,386 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The RM needs to be corrected. There is no second RCW source. This was initially planned but due to certain hardware issues, could not be implemented.

The statement should be removed:
I/O drivers for the backup RCW source are enabled, specifically those pins associated only with the secondary RCW interface.However in LX2160, we do have a provision of secondary RCW source on the same boot device. If boot fails from RCW loaded at offset 0 or 0x1000 ( in case of SD), ROM searches for RCW at 8 MB (8 Mb + 0x1000 for SD) offset on the device.