Model: NXP Layerscape LX2160ARDB Board
Board: LX2160ACE Rev2.0-RDB, Board version: C, boot from FlexSPI DEV#0
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.32.0, boot status: 0x1)
[ 4.432377] fsl_dpaa2_mac dpmac.4: Adding to iommu group 10
[ 4.444118] fsl_dpaa2_mac dpmac.4 (unnamed net_device) (uninitialized): phylink_fwnode_phy_connect() = -19
[ 4.453773] fsl_dpaa2_mac dpmac.4: Error connecting to the MAC endpoint
[ 4.460893] fsl_dpaa2_mac dpmac.4: fsl_mc_driver_probe failed: -19
[ 4.467197] fsl_dpaa2_mac dpmac.3: Adding to iommu group 10
[ 4.478894] fsl_dpaa2_mac dpmac.3 (unnamed net_device) (uninitialized): phylink_fwnode_phy_connect() = -19
[ 4.488560] fsl_dpaa2_mac dpmac.3: Error connecting to the MAC endpoint
[ 4.495692] fsl_dpaa2_mac dpmac.3: fsl_mc_driver_probe failed: -19
解決済! 解決策の投稿を見る。
It seems that there is problem with your dpl file, please modify LSDK 21.08 original DPL file dpl-eth.19.dts as the following.
/* ------------ DPNIs --------------*/
obj_set@dpni {
type = "dpni";
ids = <0x0 0x1>;
};
Modify to:
obj_set@dpni {
type = "dpni";
ids = <0x0 0x1 0x2 0x3>;
};
Then adding the following section in "Connections" section.
connection@3 {
endpoint1 = "dpni@2";
endpoint2 = "dpmac@3";
};
connection@4 {
endpoint1 = "dpni@3";
endpoint2 = "dpmac@4";
};
Thanks I will change and update.
thanks for Quick Reply and help .
After installing the dtb file getting the same error, Attached boot logs.
As per LSDK guide I will use the below command and try to load dpl file.
dtc -I dts -O dtb dpl-eth.19.dts -o dpl-eth.19.dtb
followed the below steps .
fsl-mc: Deploying data path layout ... WARNING: Firmware returned an error (GSR: 0x3f)
Can you please suggest how to solve.
It seems that there is problem with your dpl file, please modify LSDK 21.08 original DPL file dpl-eth.19.dts as the following.
/* ------------ DPNIs --------------*/
obj_set@dpni {
type = "dpni";
ids = <0x0 0x1>;
};
Modify to:
obj_set@dpni {
type = "dpni";
ids = <0x0 0x1 0x2 0x3>;
};
Then adding the following section in "Connections" section.
connection@3 {
endpoint1 = "dpni@2";
endpoint2 = "dpmac@3";
};
connection@4 {
endpoint1 = "dpni@3";
endpoint2 = "dpmac@4";
};