LSDK RFS to NOR or NAND flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK RFS to NOR or NAND flash

Jump to solution
2,287 Views
nxf47487
NXP Employee
NXP Employee

Hi

Can I use flex-builder to deploy LSDK RFS to NOR or NAND flash? I only see RFS SD/USB deployment in the document. Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,275 Views
bpe
NXP Employee
NXP Employee

I assume flex-installer was actually meant because flex-builder cannot deploy anything, it is a build automation tool. flex-installer can only deploy to a block device while NOR and NAND memories are MTD. flex-installer cannot partition such devices, so flex-builder can build a rootfs for you, but you have to deploy it by hand.

 

Have a great day,
Platon

 

View solution in original post

0 Kudos
Reply
3 Replies
2,293 Views
nxf47487
NXP Employee
NXP Employee

Deleted

0 Kudos
Reply
2,276 Views
bpe
NXP Employee
NXP Employee

I assume flex-installer was actually meant because flex-builder cannot deploy anything, it is a build automation tool. flex-installer can only deploy to a block device while NOR and NAND memories are MTD. flex-installer cannot partition such devices, so flex-builder can build a rootfs for you, but you have to deploy it by hand.

 

Have a great day,
Platon

 

0 Kudos
Reply
2,255 Views
nxf47487
NXP Employee
NXP Employee

Thanks. I mean flex-installer for the deployment.

Another question about flex-builder. Can I use flex-builder to generate jffs2 rootfs image or initramfs rootfs?

0 Kudos
Reply