LSDK RFS to NOR or NAND flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LSDK RFS to NOR or NAND flash

ソリューションへジャンプ
2,279件の閲覧回数
nxf47487
NXP Employee
NXP Employee

Hi

Can I use flex-builder to deploy LSDK RFS to NOR or NAND flash? I only see RFS SD/USB deployment in the document. Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
bpe
NXP Employee
NXP Employee

I assume flex-installer was actually meant because flex-builder cannot deploy anything, it is a build automation tool. flex-installer can only deploy to a block device while NOR and NAND memories are MTD. flex-installer cannot partition such devices, so flex-builder can build a rootfs for you, but you have to deploy it by hand.

 

Have a great day,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,285件の閲覧回数
nxf47487
NXP Employee
NXP Employee

Deleted

0 件の賞賛
返信
2,268件の閲覧回数
bpe
NXP Employee
NXP Employee

I assume flex-installer was actually meant because flex-builder cannot deploy anything, it is a build automation tool. flex-installer can only deploy to a block device while NOR and NAND memories are MTD. flex-installer cannot partition such devices, so flex-builder can build a rootfs for you, but you have to deploy it by hand.

 

Have a great day,
Platon

 

0 件の賞賛
返信
2,247件の閲覧回数
nxf47487
NXP Employee
NXP Employee

Thanks. I mean flex-installer for the deployment.

Another question about flex-builder. Can I use flex-builder to generate jffs2 rootfs image or initramfs rootfs?

0 件の賞賛
返信