LSDK 18.03: flex-installer: line 362: /run/media/sdd3/etc/hostname: Permission denied

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK 18.03: flex-installer: line 362: /run/media/sdd3/etc/hostname: Permission denied

896 Views
marje
Contributor I

I'm trying to install LSDK 18.03 images to SD card with command flex-installer under regular user:

$ flex-installer -b bootpartition_arm64_lts_4.14.tgz -r build/rfs/rootfs_ubuntu_xenial_arm64 -m ls1043ardb -d /dev/sdd

but it fails with error:

LSDK-18.03/flexbuild/tools/flex-installer: line 362: /run/media/sdd3/etc/hostname: Permission denied

I've checked the problematic line in this script.

echo "$distroname.$machine" > /run/media/${devpartname}3/etc/hostname

In this script only this line does not using sudo, but it should when modifying files on target media. It works for me, if I change this line to:

echo "$distroname.$machine" | sudo tee /run/media/${devpartname}3/etc/hostname

Does this fix make sense to you?

0 Kudos
Reply
1 Reply

624 Views
Pavel
NXP Employee
NXP Employee

Your modification is correct.

It looks like designers do not add "sudo" in this script since customer uses also different Linux versions on the host PC.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply