LS2088ardb stuck in System switches on, processor is not configured. State

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088ardb stuck in System switches on, processor is not configured. State

ソリューションへジャンプ
1,693件の閲覧回数
prafulls
Contributor II

Hi Team,

    We are using device ls2088ardb, while bootup it stuck in some unknow state, an we are unable to get the console logs from UART terminal. Also the Power led blinks in Yellow color (System switches on, processor is not configured. ).

     Can you please suggest the recovery procedure for the device.

Thanks,

Prafull

0 件の賞賛
返信
1 解決策
1,686件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try alternative RCW_SRC options referring the QorIQ LS2085A/LS2088A Reference Design Board Getting Started Guide, Table 3. Switch configurations:

1) select NOR Flash virtual bank 4

2) select QSPI

3) prepare bootable SD card and select SD 2.0

NXP LSDK reference:

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-956F22A7-1734-47B1-B...

 

元の投稿で解決策を見る

2 返答(返信)
1,687件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try alternative RCW_SRC options referring the QorIQ LS2085A/LS2088A Reference Design Board Getting Started Guide, Table 3. Switch configurations:

1) select NOR Flash virtual bank 4

2) select QSPI

3) prepare bootable SD card and select SD 2.0

NXP LSDK reference:

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-956F22A7-1734-47B1-B...

 

1,667件の閲覧回数
prafulls
Contributor II

Hi,

   Thank you for  sharing the useful information, which was very helpful to recovered ls2088ardb with given solution. 

Thanks,

Prafull

0 件の賞賛
返信