LS2088 LRDIMM configuarion support in U-boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2088 LRDIMM configuarion support in U-boot.

659 Views
vidyasagartata
Contributor II

Dear All,

This is regarding the DDR4 Memory Controller request to clarification W.R.T same, As per datasheet & RM of LS2088 Chip It supports Unbuffered and Registered DIMMs but we are planning to use Concept of LRDIMM in which RCD and Data buffer (DB) will be mounted  onboard  in order to meet Thermal and SI requirements of the design ,Kindly confirm whether LS2088 supports LRDIMM Concept.

I have gone through the ls2080ardb u-boot source code seeing LRDIMM is configured in the two files.

1). include/ddr_spd.h and driver/ddr/fsl/interactive.c.

2). If we use LRDIMM for ls2088 processor then any major modification is required in LRDIMM controller ?

Thanks,

Vidya

Labels (1)
Tags (1)
0 Kudos
1 Reply

452 Views
Bulat
NXP Employee
NXP Employee

The LS2088 does not support LRDIMMs.

Regards,

Bulat

0 Kudos