LS2080A capability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2080A capability

Jump to solution
1,937 Views
JHY
Contributor IV

Hello, experts.

LS2080A has total 16 serdes lanes for variable purpose.

So, please confirm below options are able to be implemented in LS2080A.

1. simultaneously up to 5.8G input to LS2080A and up to 2.4G output from LS2080A by PCIE.

2. vice versa 5.8G output from LS2080A and up to 2.4G input to LS2080A by PCIE

Best regards.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,707 Views
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,708 Views
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,707 Views
JHY
Contributor IV

One more question.

It has 4 PCIE controller.

Is it possible to use 2 lanes PCIE x 4 at single serdes block like below?

2x4.jpg

0 Kudos
Reply
1,707 Views
bpe
NXP Employee
NXP Employee

This is too confused. Two lanes mean PCIe x2. PCIe x4 requires four lanes. The picture displays four PCIe controllers connected

to an 8-lane SerDes, which obviously can be done in several bus width combinations. Refer to the chip Manual, Section 25.1.2.1 for available SerDes protocol combinations.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------