LS2080A capability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS2080A capability

跳至解决方案
2,375 次查看
JHY
Contributor IV

Hello, experts.

LS2080A has total 16 serdes lanes for variable purpose.

So, please confirm below options are able to be implemented in LS2080A.

1. simultaneously up to 5.8G input to LS2080A and up to 2.4G output from LS2080A by PCIE.

2. vice versa 5.8G output from LS2080A and up to 2.4G input to LS2080A by PCIE

Best regards.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,145 次查看
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,146 次查看
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,145 次查看
JHY
Contributor IV

One more question.

It has 4 PCIE controller.

Is it possible to use 2 lanes PCIE x 4 at single serdes block like below?

2x4.jpg

0 项奖励
回复
2,145 次查看
bpe
NXP Employee
NXP Employee

This is too confused. Two lanes mean PCIe x2. PCIe x4 requires four lanes. The picture displays four PCIe controllers connected

to an 8-lane SerDes, which obviously can be done in several bus width combinations. Refer to the chip Manual, Section 25.1.2.1 for available SerDes protocol combinations.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------