LS2080A - SDK-20151204-yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2080A - SDK-20151204-yocto

2,152 Views
dewantkatare
Contributor I

Hello All,

I am unable to find the SDK related to LS2080A which is released as "LS2080A-SDK-20151204-yocto.iso" file on the device software & Tools tab / SDK page.

For the development purpose, I have to install the sdk and deploy the bsp images. 

Thanks for the help and response

Labels (1)
0 Kudos
Reply
1 Reply

1,949 Views
Pavel
NXP Employee
NXP Employee

Use SDK 2.0 for QorIQ:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

 

Use 1703 patch for this SDK.

 

NXP SDK 2.0-1703 supports the ls2080ardb board. See attached screenshot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply