LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse

1,044 Views
Em31
Contributor II

Hi all,

I am trying to access theLS1046ARDB console connection from the UART to the COM by using the RJ45-to-DB9F cable.

I have changed the SW4[4] on my LS1046ARDB board to 0 and configured the teraterm configure serial speed at 115200, but there is no connection that can be established.

Could you please tell me:

1. Is there any other setup I need to configure to make it work, etc., driver?

If not, can you suggest another method to make the connection work besides connecting to the front port?

Thanks in advance.

 

0 Kudos
Reply
1 Reply

1,014 Views
Chanh
Contributor III

Hi,

For the Teraterm, did you configure all the parameters as mentioned in the Getting Start Guide?

I use an RJ45-to-USB cable instead, and it works for me. I only need to install the USB driver on my Win10 pc.

Tags (1)
0 Kudos
Reply