Hi NXP team,
We use AQR107 10G module which same with ls1046ardb.
The current situation is ...
The driver is ready (built-in kernel image) and mdio can also recognize the device.
But we still can't use it normally.
We have two questions :
1. Do we need to put firmware into AQR107's flash ? How to do it ?
2. Any RCW configuration have to check/set ?
Thanks
Best Regards,
Solved! Go to Solution.
1. Please refer to this topic
https://community.nxp.com/t5/QorIQ/Binary-for-AQR107-flash-in-LS1046ARDB/m-p/884102
2. For RCW configuration, please refer to "Table 31-1. Supported SerDes1 options" in LS1046RM, you could configure RCW[128-143] as 1133.
1. Please refer to this topic
https://community.nxp.com/t5/QorIQ/Binary-for-AQR107-flash-in-LS1046ARDB/m-p/884102
2. For RCW configuration, please refer to "Table 31-1. Supported SerDes1 options" in LS1046RM, you could configure RCW[128-143] as 1133.
Add an additional information :
We found "ERROR FM1@TGEC1 firmware loading disabled." message in booting log, what's wrong here ?
Thanks
Best Regards