LS1046A Outbound and Inbound configuration question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A Outbound and Inbound configuration question

跳至解决方案
1,548 次查看
zy_mooncity
Contributor III

Dear folks,

There is a shared memory communication scenario between two Ls1046a boards. One acts as RC and the other acts as EP. The RC Ls1046a board will access four different parts of memory located in EP Ls1046a board. Can I just configure like this: 1 outbound window, 4 inbound windows. (the outbound window is big enough to cover the total size of the 4 inbound windows. Just like a PCI RC to access different BARs in the EP)? or I have to configure 1 outbound window with 1 inbound window (4 outbound windows are needed) ?

Thanks and Regards

Yun

标签 (1)
0 项奖励
回复
1 解答
1,455 次查看
Bulat
NXP Employee
NXP Employee

1. Yes, it is necessary.

2. The ls1046a endpoint can response to the RC configuration once it's ready

Regards,

Bulat

在原帖中查看解决方案

3 回复数
1,455 次查看
Bulat
NXP Employee
NXP Employee

 It is up to you, either way can be used.

Regards,

Bulat

0 项奖励
回复
1,455 次查看
zy_mooncity
Contributor III

Hi Bulat,

Thank you for the quick response.

I have configuration questions about the Ls1046a target which acts as endpoint:

1. Is it necessary to set [CFG_READY] bit of PEX PFa Config Register (PEX_PF0_CONFIG) of Ls1046a endpoint before RC can configure it?  (I  did not find the related code in the linux driver code pcie-designware-ep.c)

2. Is it necessary to configure inbound window for the ls1046a endpoint to response CfgRd0 TLP from the RC? Or the ls1046a endpoint can response to the RC configuration once it's ready?

Thanks and Regards

Yun

0 项奖励
回复
1,456 次查看
Bulat
NXP Employee
NXP Employee

1. Yes, it is necessary.

2. The ls1046a endpoint can response to the RC configuration once it's ready

Regards,

Bulat