LS1046A - IFC GPCM Support for CSOR[ADM_SHFT_MODE] =1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A - IFC GPCM Support for CSOR[ADM_SHFT_MODE] =1

1,440 Views
CGganesh
Contributor II

Hi,

Our design is to support 20-bit addressing of IFC in GPCM mode. GPCM Mode of IFC will it support both CSOR[ADM_SHFT_MODE] 0 & 1 ? 

Regards,

Ganesh

0 Kudos
Reply
1 Reply

1,404 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello, Thank you for contacting the Technical Support Team,


Yes, it is possible if you write on the register ADM_SHFT “10100” you will have IFC with 20 bit Address,
On the other hand writing on the register ADM_SHFT_ MODE “0” or “1”you will be able to you can switch to less significant and more significant directions.


I attach some referenced images obtained from the reference manual.

Best Regards, 

Hector Villarruel S

0 Kudos
Reply