Per my system requirements I need to power down 3 of the 4 cores. Can someone point me to the documentation which discusses how to shut down the specific clocks for 3 of the 4 cores?
Thank you
Hi Daves,
I also need to disable cores in my custom LS1046a board.
I added bellow lines in components/firmware/rcw/ls1046a_custom/NN_FNSNPPPP_1133_8888/rcw_1600_qspiboot.rcw:
---
//-------------------------------------------------------------------------
// disable core 3 and 2 so we only use core 0 and 1...
.pbi
write 0x01EE0094, 0x0000000c
//write 0x01ee0094, 0x0000000e
.end
---
I rebuilt firmware_ls1046a_custom_qspiboot.img & flashed on my custom board.
But, nothing displayed in the console.
Is there anything to change more?
Regards,
Jake
Hi Jake,
My guess there's no response on the serial output is because you threw an error during the PBL portion of the boot process... The LS1046A is not very friendly if the RCW or the PBL is wrong; if the CRC doesn't match, it simply stops and sets the RESET_REQ line to reboot itself... which sends it into an endless loop if that's how your hardware is setup...
The problem with your code is the address. The commands in the PBL strip off the most significant (1) in your address, and incorporate it into the WRITE macro you're using.
If you change your PBL line to this:
.pbi
write 0x0EE0094, 0x0000000c
.end
it probably will work for you...
Hope this helps.
-Dave
Hi Scott, I just was looking into doing this myself when I ran across this unanswered question... I've sort of given up on this forum, as no one seems to respond for a really long time... looks like you asked your question over 5 months ago with no response.
Well, to show you what I did, here's a shot of my notes:
ref: 12.3.11 Core Disable Register (COREDISR)
Value Definition
0x000000002 | Core 1 disabled |
0x000000004 | Core 2 disabled |
0x000000008 | Core 3 disabled |
Values can be OR’d together to disable multiple cores.
Core 0 is always enabled…
Example:
//------------------------------------------------------------------------- // disable core 3 and 2 so we only use core 0 and 1... //------------------------------------------------------------------------- write 0xEE0094, 0x0000000C
for_each_cpu(i, core, cpu_numcores(), cpu_mask()) { if(!(i % 2)) printf("\n\t"); type = TP_ITYP_VER(fsl_qoriq_core_to_type(core)); printf("CPU%d(%s):%-4s MHz %s ", core, (type == TY_ITYP_VER_A7) ? "A7 " : (type == TY_ITYP_VER_A53 ? "A53" : (type == TY_ITYP_VER_A57 ? "A57" : (type == TY_ITYP_VER_A72 ? "A72" : " "))), strmhz(buf, sysinfo.freq_processor[core]), (in_be32(0x01EE0094) & (1<<core)) ? "[ IDLE ]" : "[ACTIVE]"); }