LS1046A DPDK L2/L3 forwarding performance with short packet(64 Bytes)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A DPDK L2/L3 forwarding performance with short packet(64 Bytes)

Jump to solution
1,429 Views
win847
Contributor I

Can LS1046A DPDK L2/L3 forwarding performance with the short packet(64 Bytes)  reach 10Mpps per core(1.8 GHz)?  What's the exact result of DPDKL2/L3 forwarding performance?

 

Does LS1046A support DMA and Cache coherency? Like description with below link:

https://abcamus.github.io/2017/06/26/ARM-CCI/

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,399 Views
yipingwang
NXP TechSupport
NXP TechSupport

We have dpdk l2fwd 10g 1core test data as the following.

FrameSize(Bytes)   Throughput(Kpps)     Throughput(Mbps)

64                                    7170                    4817.97

 

dpdk l3fwd 20g 4core performance

FrameSize(Bytes)     Throughput(Kpps)      Throughput(Mbps)     Throughput(%)

  64                              12095                              8127.73                   40.64

View solution in original post

0 Kudos
4 Replies
1,400 Views
yipingwang
NXP TechSupport
NXP TechSupport

We have dpdk l2fwd 10g 1core test data as the following.

FrameSize(Bytes)   Throughput(Kpps)     Throughput(Mbps)

64                                    7170                    4817.97

 

dpdk l3fwd 20g 4core performance

FrameSize(Bytes)     Throughput(Kpps)      Throughput(Mbps)     Throughput(%)

  64                              12095                              8127.73                   40.64

0 Kudos
1,395 Views
win847
Contributor I

Yiping, Thanks for your reply.

 

Does LS1046A support DMA and Cache coherency? 

0 Kudos
1,391 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please create a new thread for the other question.

0 Kudos
1,405 Views
win847
Contributor I

Anyone who can help to answer this question?

0 Kudos