LS1046A DPDK L2/L3 forwarding performance with short packet(64 Bytes)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A DPDK L2/L3 forwarding performance with short packet(64 Bytes)

ソリューションへジャンプ
1,406件の閲覧回数
win847
Contributor I

Can LS1046A DPDK L2/L3 forwarding performance with the short packet(64 Bytes)  reach 10Mpps per core(1.8 GHz)?  What's the exact result of DPDKL2/L3 forwarding performance?

 

Does LS1046A support DMA and Cache coherency? Like description with below link:

https://abcamus.github.io/2017/06/26/ARM-CCI/

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
1,376件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

We have dpdk l2fwd 10g 1core test data as the following.

FrameSize(Bytes)   Throughput(Kpps)     Throughput(Mbps)

64                                    7170                    4817.97

 

dpdk l3fwd 20g 4core performance

FrameSize(Bytes)     Throughput(Kpps)      Throughput(Mbps)     Throughput(%)

  64                              12095                              8127.73                   40.64

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,377件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

We have dpdk l2fwd 10g 1core test data as the following.

FrameSize(Bytes)   Throughput(Kpps)     Throughput(Mbps)

64                                    7170                    4817.97

 

dpdk l3fwd 20g 4core performance

FrameSize(Bytes)     Throughput(Kpps)      Throughput(Mbps)     Throughput(%)

  64                              12095                              8127.73                   40.64

0 件の賞賛
1,372件の閲覧回数
win847
Contributor I

Yiping, Thanks for your reply.

 

Does LS1046A support DMA and Cache coherency? 

0 件の賞賛
1,368件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a new thread for the other question.

0 件の賞賛
1,382件の閲覧回数
win847
Contributor I

Anyone who can help to answer this question?

0 件の賞賛