LS1046转发效率低LSDK-18.03

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046转发效率低LSDK-18.03

774 Views
末班车上的乘客
Contributor II

LS1046转发效率低

由综测仪到5G模组速率有3Gbps,综测仪到设备光口输出速率只有850Mbps,双设备光口对光口速率6.5Gbps

SDK:LSDK-18.03

操作系统:ubuntu18.04.1 LTS

5G模块接口:USB3.0

核心板:飞凌OK1046

Tags (1)
0 Kudos
Reply
1 Reply

760 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following 4core 20g IP fwd test result on LS1046ARDB with LSDK 1803 Kernel 4.14.

SessID CaseName TagVersion PlatformType OSType BoardName1 SiVer1 CDCF1 MC1 CPUQuantity1 BoardName2 SiVer2 CDCF2 MC2 CPUQuantity2 Username Notes Testitem PassRate ThroughputKpps ThroughputMbps  
29280 linux_ipv4_fwd_4c20g_b2b_perf lsdk-1803-tc2-v4.14 LS1046ARDB 64bit LS1046ARDB-2 1.0 1800/2100/700/800 8 GiB 4       NA NA   NA 64 6.64 1975 1327.29    
128 11.9 2011 2380.92    
256 21.07 1909 4215.02    
390 31.22 1904 6244.24    
512 42.24 1985 8449.06    
1024 79.22 1897 15844.0    
1280 93.46 1797 18692.71    
1518 64.59 1050 12917.25    
0 Kudos
Reply