LS1043a-rdb network problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043a-rdb network problem

跳至解决方案
2,094 次查看
eriktideman
Contributor III

We are using the LS1043a-rdb -pa evaluation board and having problem with ethernet in linux. When we build the kernel with the SDK-2.0's defconfig (kernel version 4.1.8) none of the ethernet interfaces RX counter increases despite connected to whatever other network equipment. TX works fine.

When switching kernel to the SDK-0.5's defconfig (kernel version 3.19) all interfaces works fine. Is there any configuration in the latest SDK that we are missing?

标签 (1)
0 项奖励
回复
1 解答
1,875 次查看
Pavel
NXP Employee
NXP Employee

Usually similar problem happens if there is no FMAN microcode. Check your boar using the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-A83D8AAA-27F0-4E9A-BFC5-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-4BF3D3AB-4098-432C-820B-4...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-929B4381-1F81-4B48-B378-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-395614F4-A733-4219-BB1D-8...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,876 次查看
Pavel
NXP Employee
NXP Employee

Usually similar problem happens if there is no FMAN microcode. Check your boar using the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-A83D8AAA-27F0-4E9A-BFC5-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-4BF3D3AB-4098-432C-820B-4...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-929B4381-1F81-4B48-B378-C...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-395614F4-A733-4219-BB1D-8...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,875 次查看
eriktideman
Contributor III

Thanks, I were not aware of this and will look at it!

Regards Erik.

0 项奖励
回复