LS1043ARDB-PA/PB evaluation board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB-PA/PB evaluation board.

Jump to solution
1,118 Views
trondwang
Contributor I

Hi,

in the schematic diagram of the evaluation board there is a power U46 that creates a voltage (S1VDD_SRC) that not seems to be connected.

What is the reason for this power?

thanks and regards,

Trond Inge#

Labels (1)
0 Kudos
1 Solution
806 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Some revisions of the LS1043ARDB-PA have the LS1043A S1VDD powered from the U46.

S1VDD_SRC.png
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
807 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Some revisions of the LS1043ARDB-PA have the LS1043A S1VDD powered from the U46.

S1VDD_SRC.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos