LS1043ARDB: P4 PCIe-x1 extension cable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB: P4 PCIe-x1 extension cable

246件の閲覧回数
ts1234
Contributor III
I am trying to use a PCIe-x1 device on P4 of the LS1043ARDB, with the help of a PCIe-x1 extension cable, but I am getting the continuous stream of the following kernel errors. 
How do I fix this? (Device works without the extension cable. This cable works on PC)
 
[  161.320269] pcieport 0001:00:00.0: AER:   device [1957:8080] error status/mask=00000001/00006000
[  161.329059] pcieport 0001:00:00.0: AER:    [ 0] RxErr
[  161.335592] pcieport 0001:00:00.0: AER: Multiple Corrected error received: 0001:00:00.0
[  161.343604] pcieport 0001:00:00.0: AER: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  161.353607] pcieport 0001:00:00.0: AER:   device [1957:8080] error status/mask=00000001/00006000
[  161.362399] pcieport 0001:00:00.0: AER:    [ 0] RxErr
[  161.368930] pcieport 0001:00:00.0: AER: Multiple Corrected error received: 0001:00:00.0
[  161.376944] pcieport 0001:00:00.0: AER: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
 
0 件の賞賛
0 返答(返信)