LS1043A can not find MAC address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A can not find MAC address

ソリューションへジャンプ
1,462件の閲覧回数
Hahawell
Contributor III

Hi, Expert:

    Our software and hardware come from LS1043ARDB. We deleted CPLD and keeps the same PHY IC(RTL8211FS).and we try to stay in step with the LS1043ARDB。

  Our problems are:

  1)We can not get MAC address automatically;

  2)We write the fixed MAC address in software.and We notice that it can ping the PC under uboot mode but it can not ping  the PC under Linux system,and We get the message“connect: Network is unreachable”

 We hope somebody can give us some advices.

 Thank you!

タグ(1)
0 件の賞賛
返信
1 解決策
1,452件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In u-boot, please configure environment variables as the following

eth10addr=00:E0:0C:00:2B:0a
eth11addr=00:E0:0C:00:2B:0b
eth12addr=00:E0:0C:00:2B:0c
eth13addr=00:E0:0C:00:2B:0d
eth14addr=00:E0:0C:00:2B:0e
eth15addr=00:E0:0C:00:2B:0f
eth1addr=00:E0:0C:00:2B:01
eth2addr=00:E0:0C:00:2B:02
eth3addr=00:E0:0C:00:2B:03
eth4addr=00:E0:0C:00:2B:04
eth5addr=00:E0:0C:00:2B:05
eth6addr=00:E0:0C:00:2B:06
eth7addr=00:E0:0C:00:2B:07
eth8addr=00:E0:0C:00:2B:08
eth9addr=00:E0:0C:00:2B:09
ethaddr=00:E0:0C:00:2B:00

In u-boot, would you please provide the result of command "mdio list"?

=> mdio list
FSL_MDIO0:
1 - RealTek RTL8211F <--> FM1@DTSEC3
2 - RealTek RTL8211F <--> FM1@DTSEC4
4 - Vitesse VSC8514 <--> FM1@DTSEC1
5 - Vitesse VSC8514 <--> FM1@DTSEC2
6 - Vitesse VSC8514 <--> FM1@DTSEC5
7 - Vitesse VSC8514 <--> FM1@DTSEC6
FM_TGEC_MDIO:
1 - Aquantia AQR105 <--> FM1@TGEC1

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,453件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In u-boot, please configure environment variables as the following

eth10addr=00:E0:0C:00:2B:0a
eth11addr=00:E0:0C:00:2B:0b
eth12addr=00:E0:0C:00:2B:0c
eth13addr=00:E0:0C:00:2B:0d
eth14addr=00:E0:0C:00:2B:0e
eth15addr=00:E0:0C:00:2B:0f
eth1addr=00:E0:0C:00:2B:01
eth2addr=00:E0:0C:00:2B:02
eth3addr=00:E0:0C:00:2B:03
eth4addr=00:E0:0C:00:2B:04
eth5addr=00:E0:0C:00:2B:05
eth6addr=00:E0:0C:00:2B:06
eth7addr=00:E0:0C:00:2B:07
eth8addr=00:E0:0C:00:2B:08
eth9addr=00:E0:0C:00:2B:09
ethaddr=00:E0:0C:00:2B:00

In u-boot, would you please provide the result of command "mdio list"?

=> mdio list
FSL_MDIO0:
1 - RealTek RTL8211F <--> FM1@DTSEC3
2 - RealTek RTL8211F <--> FM1@DTSEC4
4 - Vitesse VSC8514 <--> FM1@DTSEC1
5 - Vitesse VSC8514 <--> FM1@DTSEC2
6 - Vitesse VSC8514 <--> FM1@DTSEC5
7 - Vitesse VSC8514 <--> FM1@DTSEC6
FM_TGEC_MDIO:
1 - Aquantia AQR105 <--> FM1@TGEC1

0 件の賞賛
返信