LS1043A: Marvell 88e6141 on SerDes Lane B and EMI1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A: Marvell 88e6141 on SerDes Lane B and EMI1

Jump to solution
3,170 Views
MaxLiou
Contributor II

Hello

We have a custom designed board based on the LS1043A, which has a Marvell 88e6141 switch connected to SerDes lane B and EMI1.
The SerDes configuration is 0x2255.
Due to we're very similar to below case:
https://community.nxp.com/t5/Layerscape/LS1043A-Marvell-88e6341-on-SerDes-lane-B-and-EMI1-EC1/m-p/11...
I modify a dts file based on above case.

On booting log, OS can recognize switch.
But still can't ping via switch.

Also upload my /etc/config/network setting, in case the setting is wrong.

Would you please tell me which part is wrong? dts or network setting?

Best regards,
Max Liou

0 Kudos
1 Solution
3,140 Views
MaxLiou
Contributor II

Dear Yiping,

I have try three different compatible as below:

"marvell,mv88e6141", "marvell,mv88e6341" and "marvell,mv88e6085" (all in Boot_Log.zip).

Only "marvell,mv88e6085" can find "switch 0x3400 detected: Marvell 88E6341" and "entered forwarding state" in boot log.

And refer to \linux-4.14.202\Documentation\devicetree\bindings\net\dsa\marvell.txt, it also describes should be one of "marvell,mv88e6085" or
"marvell,mv88e6190".

But even the switch enter forwarding state, I still can't ping to my laptop.

There's only TX's data increases, RX's bytes remains 0 (0.0 B)

Am I wrong in my /etc/config/network setting?

(Block  diagram of PHY/switch also upload) 

View solution in original post

0 Kudos
6 Replies
3,153 Views
MaxLiou
Contributor II

Dear Yiping, 

Thanks for your promptly response.

I forgot to write our openwrt info:

OpenWRT version : 19.07

Kernel version : 4.14.202

 

Due to we're not using "extirq 11", I change to use our interrupt  interrupts = <0 132 IRQ_TYPE_LEVEL_HIGH>

Unfortunately, I still can't get any RX data on eth1.

Upload boot log as attachment.

BR,

Max

0 Kudos
3,148 Views
yipingwang
NXP TechSupport
NXP TechSupport

Have you tried the following configuration?

mdio: mdio@fc000 {
switch0: switch0@0 {
compatible = "marvell,mv88e6141";

0 Kudos
3,141 Views
MaxLiou
Contributor II

Dear Yiping,

I have try three different compatible as below:

"marvell,mv88e6141", "marvell,mv88e6341" and "marvell,mv88e6085" (all in Boot_Log.zip).

Only "marvell,mv88e6085" can find "switch 0x3400 detected: Marvell 88E6341" and "entered forwarding state" in boot log.

And refer to \linux-4.14.202\Documentation\devicetree\bindings\net\dsa\marvell.txt, it also describes should be one of "marvell,mv88e6085" or
"marvell,mv88e6190".

But even the switch enter forwarding state, I still can't ping to my laptop.

There's only TX's data increases, RX's bytes remains 0 (0.0 B)

Am I wrong in my /etc/config/network setting?

(Block  diagram of PHY/switch also upload) 

0 Kudos
3,164 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try the following dts configuration.

mdio: mdio@fc000 {
switch0: switch0@0 {
compatible = "marvell,mv88e6341"; /*JL<M>*/
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;

interrupts-extended = <&extirq 11 IRQ_TYPE_LEVEL_LOW>;
reset-gpios = <&gpio3 15 GPIO_ACTIVE_LOW>;

0 Kudos
2,502 Views
yanglili
Contributor I

SerDes Lane A is xfi

The probing of the Marvell chip fails late with error -517. The problem seems to be that somehow the reference from the CPU port to the ethernet interface is not working. Function dsa_port_parse_of in dsa2.c fails because of_find_net_device_by_node(ethernet); returns NULL.

LSDK:2108

ethernet@f0000 {
fixed-link = <6 1 10000 0 0>;
phy-connection-type = "10gbase-kr";
};

mdio1:mdio@fd000 {
switch0: switch0@6 {
compatible = "marvell,mv88e6190";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x6>;
interrupts-extended = <&extirq 10 IRQ_TYPE_LEVEL_LOW>;
dsa,member = <0 0>;

ports {
#address-cells = <1>;
#size-cells = <0>;

port@0 {
reg = <0>;
label = "cpu";
fixed-link = <6 1 10000 0 0>;
ethernet = <&enet6>;
local-mac-address = [42 00 00 00 00 80];
fixed-link {
speed = <10000>;
full-duplex;
};
};

static int dsa_port_parse_of(struct dsa_port *dp, struct device_node *dn)
{
struct device_node *ethernet = of_parse_phandle(dn, "ethernet", 0);
const char *name = of_get_property(dn, "label", NULL);
bool link = of_property_read_bool(dn, "link");

dp->dn = dn;

if (ethernet) {
struct net_device *master;

master = of_find_net_device_by_node(ethernet);
if (!master)
return -EPROBE_DEFER;

return dsa_port_parse_cpu(dp, master);
}

if (link)
return dsa_port_parse_dsa(dp);

return dsa_port_parse_user(dp, name);
}

0 Kudos
2,426 Views
JonatanRuiz
Contributor I

Hi Yangili,

The same happens to me...

Debugging the startup process I figure out that the ethernet device you have to link to the switch is the on in: arch/arm64/boot/dts/freescale/qoriq-dpaa-eth.dtsi

fsldpaa: fsl,dpaa {
	compatible = "fsl,ls1043a-dpaa", "simple-bus", "fsl,dpaa";
	ethernet@0 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet0>;
		dma-coherent;
	};
	ethernet@1 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet1>;
		dma-coherent;
	};
	ethernet@2 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet2>;
		dma-coherent;
	};
	ethernet@3 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet3>;
		dma-coherent;
	};
	ethernet@4 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet4>;
		dma-coherent;
	};
	ethernet@5 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet5>;
		dma-coherent;
	};
	switch_cpu_port: ethernet@8 {
		compatible = "fsl,dpa-ethernet";
		fsl,fman-mac = <&enet6>;
		dma-coherent;
	};
};

Add a label to the port you want to use "switch_cpu_port"

Add also a label to the port you defined on the switch as CPU one, for example "cpu_ethernet: port@0 {...".

And assign it on the arch/arm64/boot/dts/freescale/fsl-ls1043a-<YOUR BOARD>-sdk.dts

&cpu_ethernet {
    ethernet = <&ethernet_switch>;
};

 

This solution worked for me. Good luck!

 

0 Kudos