LS1043A MDC/MDIO AC timing sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A MDC/MDIO AC timing sequence

Jump to solution
1,444 Views
shawn_tao
Contributor I

LS1043A 中EMI1_MDC/MDIO接口时序问题:

根据手册147页的示意图,写时序:EMI1在MDC上升沿延迟tMDKHDX后数据翻转,但是示波器实际测量MDC是在下降沿打出数据,如下图:这是手册描述问题还是有什么配置呢?

pastedImage_1.png

另外,读时序时:PHY在MDC的上升沿经过一段延迟后扇出数据,CPU也是利用这个上升沿采样吗?还是可以配置CPU使用下降沿采样?

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,338 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Data Path Acceleration Architecture (DPAA) Reference Manual.

View solution in original post

0 Kudos
3 Replies
1,338 Views
ufedor
NXP Employee
NXP Employee

MDIO behaviour in the provided trace is valid.

Please check MDC to MDIO delay tMDKHDX controlled by the MDIO_CFG[MDIO_HOLD].

Please check whether MDIO_CFG[NEG]=1 then LS1043A will transmit data on falling edge of the clock.

This implies with MDIO_CFG[NEG]=1 the tMDKHDX should be measured with respect to the falling edge of clock.

> can I configure the CPU to use falling edge sampling?

No.

0 Kudos
1,338 Views
shawn_tao
Contributor I

where could I find these registers in the doc: QorIQ LS1043A Reference Manual Rev. 4, 6/2018.

Thanks.

0 Kudos
1,339 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Data Path Acceleration Architecture (DPAA) Reference Manual.

0 Kudos