LS1043A: How to set Marvell 88e6141 on SerDes Lane B ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A: How to set Marvell 88e6141 on SerDes Lane B ?

Jump to solution
1,247 Views
MaxLiou
Contributor II

Dear NXP,

I have a question about "shall I do any setting on SERDES Lane B?"

 

HW Condition as below:

We have a custom designed board based on the LS1043A, which has a Marvell 88e6141 switch connected to SerDes lane B and EMI1.
The SerDes configuration is 0x2255.

0 Kudos
Reply
1 Solution
1,238 Views
ufedor
NXP Employee
NXP Employee

No additional configuration settings for SerDes are needed considering that correct RCW and SerDes reference clock are applied.

View solution in original post

0 Kudos
Reply
1 Reply
1,239 Views
ufedor
NXP Employee
NXP Employee

No additional configuration settings for SerDes are needed considering that correct RCW and SerDes reference clock are applied.

0 Kudos
Reply