Hi,
unfortunately I have no possibility to connect the pins on my voltage regulator and I have found various recommendations....
AN5012 from 2016 recommend "This pins should be left floating" if not used,
and for LS1046
5) As I already wrote: "If not used could be left unconnected."
Hi @netzocep,
Kindly use the latest revision of document for your design which is available at the NXP site. And as per the latest revision design checklist, the pins should not be left floating. You can go through the LS1046A FRWY schematic design for further reference.
Regards,
Mrudang
Dear Mrudang,
I knew the schematic, a Buck Regulator with a differential / Kelvin sense option is used.
You assume that it is absolutely necessary to use a DC/DC Buck regulator for the core voltage with a differential sense amplifier?
regards
Hi,
at the LS1046 FRWY design the part LTC7150S with a sense Pin is used (Vout-/ pin A6),
For my design with the LS1043 the LTC7150S is oversized (20Amps), I would like to use the
the LT8642EV-1 (10Amps).
regards
Hi,
I would like to use a DC/DC Buck without a differential sense amplifier, means "not used" Pins, table 4 / AN5012. Is it ok to float VDDSENSE and GNDSENSE, or do I need a DC/DC Buck with a differential sense amplifier?
regards