LS1043, VDDSENSE, GNDSENSE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043, VDDSENSE, GNDSENSE

5,026 Views
netzocep
Contributor I

Hi, do I need to connect the SENSEVDD and SENSEGND Pins? How to terminate when unused? thanks

0 Kudos
Reply
16 Replies

4,977 Views
netzocep
Contributor I

Hi,

unfortunately I have no possibility to connect the pins on my voltage regulator and I have found various recommendations....

AN5012 from 2016 recommend "This pins should be left floating" if not used, 

and for LS1046

<https://community.nxp.com/t5/QorIQ/LS1046A-Inquiries-regarding-pin-termination/m-p/1154382/highlight...>

5) As I already wrote: "If not used could be left unconnected."

0 Kudos
Reply

4,962 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

Kindly use the latest revision of document for your design which is available at the NXP site. And as per the latest revision design checklist, the pins should not be left floating. You can go through the LS1046A FRWY schematic design for further reference.

Regards,
Mrudang

0 Kudos
Reply

4,956 Views
netzocep
Contributor I

Dear Mrudang,

I knew the schematic, a Buck Regulator with a differential / Kelvin sense option is used.

You assume that it is absolutely necessary to use a  DC/DC Buck regulator for the core voltage with a differential sense amplifier?

 

regards

 

0 Kudos
Reply

4,954 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

Refer to LS1046A FRWY design as it doesn't have the sense pin. Can you share the mfg part no. of the regulator that you intended to use?

Regards,
Mrudang

0 Kudos
Reply

4,951 Views
netzocep
Contributor I

Hi,

at the LS1046 FRWY design the part LTC7150S with a sense Pin is used (Vout-/ pin A6),

For my design with the LS1043 the LTC7150S is oversized (20Amps), I would like to use the 

the LT8642EV-1 (10Amps).

regards

0 Kudos
Reply

4,898 Views
netzocep
Contributor I

Hi, 

any news to my reply?

regards

0 Kudos
Reply

4,751 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

Please connect the VDDSENSE to the VDD rail. Ensure the pin don't left floating.

Regards,
Mrudang

0 Kudos
Reply

4,744 Views
netzocep
Contributor I

Hi,

thanks, and GNDSENSE to GND rail?

regards

0 Kudos
Reply

4,739 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

Yes, connect to GND.

Regards,
Mrudang

0 Kudos
Reply

4,893 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

I am working on your case and I will get back to you once I have any progress.

I hope you understand

Regards,
Mrudang

0 Kudos
Reply

4,890 Views
netzocep
Contributor I

perfect

0 Kudos
Reply

5,019 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep 


Refer to table#4 in AN5012 for the termination details of SENSEVDD & SENSEGND pins.

Regards,
Mrudang Shelat

0 Kudos
Reply

5,014 Views
netzocep
Contributor I

Hi,

I would like to use a DC/DC Buck without a differential sense amplifier, means "not used" Pins, table 4 / AN5012. Is it ok to float VDDSENSE and GNDSENSE, or do I need a DC/DC Buck with a differential sense amplifier?

regards

0 Kudos
Reply

5,011 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

If not used then connect to regulator feedback as per the AN5012.

Regards,
Mrudang

0 Kudos
Reply

5,003 Views
netzocep
Contributor I

sorry, Is it ok to float VDDSENSE and GNDSENSE?, with the buck regulator I would like to use there is no possibility to connect these pins to the DC/DC Buck regulator feedback.

regards

0 Kudos
Reply

4,999 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @netzocep,

These pins should not be left floating. I suggest you to follow the design checklist of LS1043A.

Regards,
Mrudang

0 Kudos
Reply