LS1043 RCW CRC is different from my calculation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 RCW CRC is different from my calculation

Jump to solution
915 Views
thehk
Contributor II

Hello everybody, 

i am using LS1043ardb demo board, in PBL i tried to calculate and verify CRC at the end of the PBI END command. However it is different from what i calculated. I used more than one tool to calculate it so i don't think that it is a calculation mistake. The procedure that i follow, i collect all the memory region from beginning of the RCW data (0x6000_0000) to end of the END command which is located in PBI section. (except CRC i took all of them). But CRC is different where is my mistake?

Thank you for your interesting.

Tags (3)
0 Kudos
Reply
1 Solution
881 Views
June_Lu
NXP TechSupport
NXP TechSupport

Try to use generate correct binaries with command below with Layerscape Linux Distribution POC User Guide, Rev. L5.15.71-2.2.0 5.2.3.1 How to compile PBL binary from RCW source file

  1. $ git clone https://github.com/nxp-qoriq/rcw
  2. $ cd rcw
  3. $ git checkout -b LSDK-21.08 LSDK-21.08
  4.  $ cd ls1043x
  5.  If required, make changes to the rcw files.
  6.  $ make

View solution in original post

1 Reply
882 Views
June_Lu
NXP TechSupport
NXP TechSupport

Try to use generate correct binaries with command below with Layerscape Linux Distribution POC User Guide, Rev. L5.15.71-2.2.0 5.2.3.1 How to compile PBL binary from RCW source file

  1. $ git clone https://github.com/nxp-qoriq/rcw
  2. $ cd rcw
  3. $ git checkout -b LSDK-21.08 LSDK-21.08
  4.  $ cd ls1043x
  5.  If required, make changes to the rcw files.
  6.  $ make