LS1043 EXTENDED RCW PIN MUX SETTINGS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 EXTENDED RCW PIN MUX SETTINGS

1,100 Views
nikhilprakash
Contributor IV

Hi,

I am currently working on LS1043ardb reference board.I want to access USB2_DRVVBUS,USB2_PWRFAULT,USB3_DRVVBUS which is an alternate functionality of IIC3 and IIC4.Can anyone suggest me on how to set extended rcw pin mux register.Please help.

Thanks in advance

Labels (1)
1 Reply

747 Views
r8070z
NXP Employee
NXP Employee

May be you mean what values should be set to the Extended RCW PinMux Control Register for required configuration?

It is supposed that on the LS1043ardb USB2_DRVVBUS USB2_PWRFAULT should be configured when system has started. Check SW3[7] settings (default should be 1). LS1043A I2C2, I2C3, and I2C4 are not used, to simplify the circuit and save many mux/demux parts, LS1043ARDB attach all I2C devices to I2C1 port.