LS1028a reset fuses to '0' in development mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1028a reset fuses to '0' in development mode?

909 次查看
mbourhis
Contributor II

Hi,

I am currently working on the SecureBoot for my board.

During the step of 'development' or 'testing',

is there a way to reset or set to '0' the SRKH fuses, after they have been blown

by the command 'mw 0x01e80020 0x2' (write '0x2' in the SFP_INGR register).

 

Or maybe, is there a way to 'test' the SecureBoot without blow the SRHK fuses?

 

Thank you for your help.

Best regards,

 

Mikael Bourhis

标记 (1)
0 项奖励
回复
1 回复

899 次查看
ufedor
NXP Employee
NXP Employee

> is there a way to reset or set to '0' the SRKH fuses, after they have been blown

There is no such way.

> is there a way to 'test' the SecureBoot without blow the SRHK fuses?

Please refer to the Layerscape Software Development Kit User Guide, 6.1.1.5.2.4.1 Program SRKH mirror registers in CodeWarrior environment, 4. Platform LS1028A (TA 3.x).

 

0 项奖励
回复