[LS1028A] : Unable to boot u-boot from FlexSPI flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1028A] : Unable to boot u-boot from FlexSPI flash

1,945件の閲覧回数
Arathi
Contributor II

Hi @nxp support Team,

We are working with NXP LS1028A processor connected to 32 bit DDR4 + 4bit ECC(MT40A1G16KH-062E) and FlexSPI NOR Flash (MT35XU01GBBA1G12).

In JTAG mode I am able to connect to code warrior Flash prompt and load the generated images into NOR flash as shown below

Arathi_0-1723028017133.png

When i am trying to boot from NOR Flash it is getting stuk after bl31 phase with the print NOTICE: Welcome to LS1028 BL31 Phase

Arathi_1-1723028061334.png

I able to connect to DDR validation tool of CodeWarrior Development studio. Tried running validation and operation test for DDR4 with 800MHz speed and found both to be passed. Configured the generated DDR config parameters into uboot ddr_init.c file in the path packages/firmware/atf/plat/nxp/soc-ls1028/ls1028ardb/ddr_init.c .

Attaching the generated ddr config file for your reference

still observed the uboot to get stuck after bl31 phase.

Pls do help us to boot LS1028A from NOR flash and let us know what else has to be done for the same.

Thanks and Regards,
Arathi

0 件の賞賛
返信
5 返答(返信)

1,683件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

Apologies for the delayed response,

Just to let you know that I still waiting a response from the specialist team, When I have any update I will let you know

Regards,

0 件の賞賛
返信

1,814件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am in touch with a team of specialists regarding your enquiry. As soon as I receive any updates, I will let you know.

Regards

0 件の賞賛
返信

1,838件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am in touch with a team of specialists regarding your enquiry. As soon as I receive any updates, I will let you know.

0 件の賞賛
返信

1,926件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am already working on your issue, When I have any update,

Regards

0 件の賞賛
返信

1,856件の閲覧回数
Arathi
Contributor II

Hi @SebastianG 

Any update on the above issue.

As this is the starting stage of bringup please consider this on priority.

Please do let us know if you have anything else to be tried.

Thanks
Arathi

0 件の賞賛
返信