[LS1028A] : Unable to boot u-boot from FlexSPI flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1028A] : Unable to boot u-boot from FlexSPI flash

1,869 Views
Arathi
Contributor II

Hi @nxp support Team,

We are working with NXP LS1028A processor connected to 32 bit DDR4 + 4bit ECC(MT40A1G16KH-062E) and FlexSPI NOR Flash (MT35XU01GBBA1G12).

In JTAG mode I am able to connect to code warrior Flash prompt and load the generated images into NOR flash as shown below

Arathi_0-1723028017133.png

When i am trying to boot from NOR Flash it is getting stuk after bl31 phase with the print NOTICE: Welcome to LS1028 BL31 Phase

Arathi_1-1723028061334.png

I able to connect to DDR validation tool of CodeWarrior Development studio. Tried running validation and operation test for DDR4 with 800MHz speed and found both to be passed. Configured the generated DDR config parameters into uboot ddr_init.c file in the path packages/firmware/atf/plat/nxp/soc-ls1028/ls1028ardb/ddr_init.c .

Attaching the generated ddr config file for your reference

still observed the uboot to get stuck after bl31 phase.

Pls do help us to boot LS1028A from NOR flash and let us know what else has to be done for the same.

Thanks and Regards,
Arathi

0 Kudos
Reply
5 Replies

1,607 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

Apologies for the delayed response,

Just to let you know that I still waiting a response from the specialist team, When I have any update I will let you know

Regards,

0 Kudos
Reply

1,738 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am in touch with a team of specialists regarding your enquiry. As soon as I receive any updates, I will let you know.

Regards

0 Kudos
Reply

1,762 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am in touch with a team of specialists regarding your enquiry. As soon as I receive any updates, I will let you know.

0 Kudos
Reply

1,850 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @Arathi,

I am already working on your issue, When I have any update,

Regards

0 Kudos
Reply

1,780 Views
Arathi
Contributor II

Hi @SebastianG 

Any update on the above issue.

As this is the starting stage of bringup please consider this on priority.

Please do let us know if you have anything else to be tried.

Thanks
Arathi

0 Kudos
Reply