LS1028A ENETC does not transmitt.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A ENETC does not transmitt.

854 Views
rhaas
Contributor IV

I am writing ENETC support for a bare-bones project (LS1028A). I am using u-boot fsl_enetc.c as an example. Whenever I try to transmit the controller seems to not acknowledge the packet.

I have rechecked my code that was based on the u-boot fsl_enetc.c file. I don’t see anything I am missing. When I transmit, the enetc controller doesn’t seem to process the buffer descriptor I present to it.

FYI, the RCW I am using are the same as the NXP dev board values. Here are my initialization steps:

  1. I issue an PCIe FLR by writing 0x8000 to 0x1F0000048 (PCI_CFC_PCIE_DEV_CTL). I wait 100 msec.
  2. I set 0x1F0000004 (PCI_CFH_CMD) to 0x406.
  3. I set SGMIIACR1 to 0x800 to enable SGMII on the SERDES.
  4. I initialize the SGMII interface using the MDIO registers (PM0_MDIO_CFG, PM0_MDIO_CTL, and PM0_MDIO_DATA). This was based on the u-boot code. I verified the writes are working by reading the values back.
  5. I setup the MAC address using PSI0PMAR0 and PSI0MAR1.
  6. I setup the RX and TX BDR count both to one using  PSI0CFGR0.
  7. I set the max packet frame size to 1536 using PM0_MAXFRM.
  8. I enable the MAC port by writing 0x8813 to PM0_COMMAND_CONFIG. This is the same value used in u-boot.
  9. I enable the port by writing a 0x10000 to PMR.
  10. I write a 0x30303030 to SICAR0. The value is different from u-boot because the MMU and cache are not enabled.
  11. I enable the station interface by writing a 0x80000000 to SIMR.

To setup the TX buffer descriptors I followed the u-boot code. I made sure the descriptors are 128 byte aligned. I printed out the contents of the descriptor and everything seems ok. However when I increment TB0PIR, I never see TB0CIR change. It is as if the controller isn’t started.

I am not using the MMU or cache with this code. I do not know if that is an issue.

I am not using a PCIe driver to discover the Ethernet controller since the addresses and capabilities are hardcoded.

Any suggestions why I can’t transmit would be helpful.

0 Kudos
Reply
2 Replies

808 Views
June_Lu
NXP TechSupport
NXP TechSupport

Sorry to late reply due to OoO.

Any update for this case?

0 Kudos
Reply

804 Views
rhaas
Contributor IV

We decided to purchase assistance from the ProSupport Team. If I find out what I am doing wrong, I will try to post it here.

Thank you for your response.

0 Kudos
Reply