LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout

ソリューションへジャンプ
2,067件の閲覧回数
igor_franco
Contributor IV

Hello,

We are using the LS1027AE processor in a custom board with a DDR3 (IS43/46TR16256BL-125K). We are trying to program its eMMC with the CodeWarrior. First, we try to run the diagnostic routine to see if is everything OK. After executing it, the target initialization script fails due to D_INIT timeout (ERR_DETECT = 0x80), making the "Test DDR memory access" failing it too. See the image below:

TARGET_INIT.PNG

Could someone help me to understand where our mistake is?

Obs.: Find our target initialization file, the DDR datasheet, and the CCS log (with log v) attached to this post.

Best regards,
Igor

0 件の賞賛
1 解決策
2,055件の閲覧回数
ufedor
NXP Employee
NXP Employee

Flash Programmer can operate even if DDR SDRAM is not initialized.

Please use the CodeWarrior QCVS DDR Tool wizard and provide screenshot of the filled DDR configuration (refer to the attached).

Please provide the processor connection schematics as PDF for inspection.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
2,056件の閲覧回数
ufedor
NXP Employee
NXP Employee

Flash Programmer can operate even if DDR SDRAM is not initialized.

Please use the CodeWarrior QCVS DDR Tool wizard and provide screenshot of the filled DDR configuration (refer to the attached).

Please provide the processor connection schematics as PDF for inspection.

0 件の賞賛
1,960件の閲覧回数
igor_franco
Contributor IV

Hello ufedor,

Sorry for the late reply.

Using the DDR Tool Wizard, we were able to configure and program our eMMC device.

Thank you for your help.

Best regards,

Igor

0 件の賞賛