LS1021atwr slow boot time from norflash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021atwr slow boot time from norflash

455 次查看
Weidonggui
Contributor I

I am using LSDK2012 to generate the boot firmware and verify it on the LS1021atwr board. The uboot version used by LSDK2012 is 2020.04. The board is powered on and booted from norflash. It takes about 15s to print information on the debugging serial port, and I use the same version of uboot After booting from SD card, the boot information is output soon, so what is the problem?

0 项奖励
1 回复

423 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I didn't reproduce this problem on my LS1021ATWR.

I used u-boot image from LSDK 21.08.

U-Boot 2021.04-ge2eba0cd58 (Aug 27 2021 - 21:50:31 +0800)

0 项奖励