LS1021a-TWR PCIe linux driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021a-TWR PCIe linux driver

跳至解决方案
1,393 次查看
jasonhendrix
Contributor V

In the QorIQ SDK documentation, the Linux driver section 7.11 references the MPC85xx platform and Linux 3.19.3 or later.  Is there a pcie Linux driver for the LS1021A-TWR?

标签 (1)
标记 (4)
0 项奖励
1 解答
1,050 次查看
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

在原帖中查看解决方案

0 项奖励
1 回复
1,051 次查看
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

0 项奖励