LS1021A - USB 3.0 as USB 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A - USB 3.0 as USB 2.0

Jump to solution
871 Views
asdwqe871188
Contributor I

Hi,

We want to use USB to Mirco SD card IC(USB2244) for storage (not boot).

My question is can I just connect the USB2.0 part (USB1_D_M/P) of the USB3.0 PHYs to USB2244?

Are there any incompatibility issues?

or you can recommend other ICs that can be used?

Thanks.

0 Kudos
Reply
1 Solution
854 Views
Pavel
NXP Employee
NXP Employee

USB 3.0 is backwards-compatible with USB 2.0.

USB 2.0 device can be connected to USB 3.0 host. There are no problems for this connection.

See USB 3.0 Specification about compatibility to USB 2.0 device.

See also the following page:

https://www.researchgate.net/publication/276931934_Brief_about_USB_30_and_Comparison_with_USB_20

View solution in original post

0 Kudos
Reply
1 Reply
855 Views
Pavel
NXP Employee
NXP Employee

USB 3.0 is backwards-compatible with USB 2.0.

USB 2.0 device can be connected to USB 3.0 host. There are no problems for this connection.

See USB 3.0 Specification about compatibility to USB 2.0 device.

See also the following page:

https://www.researchgate.net/publication/276931934_Brief_about_USB_30_and_Comparison_with_USB_20

0 Kudos
Reply